- Home - Belden.com
- About Belden
-
Market Solutions
-
Products
-
Resource Center
St. Louis, Missouri - January 31, 2012 —
Belden Inc. (NYSE:BDC), a global leader in signal transmission solutions for mission-critical applications, has added a modular industrial patch panel (MIPP) to its Belden and Hirschmann product series. The new MIPP is a termination panel for cables that need to be connected to active equipment such as switches, Industrial Ethernet devices and any other device with an Ethernet link. The MIPP offers greater system reliability and ease of installation and provides the ideal connection between Belden cables and Hirschmann switches. Its design is similar to the Hirschmann range of products.
Using patchcords to connect to active equipment, cables can be terminated outside the cabinet in an organized and structured manner to ensure the highest level of reliability. Installation is quick and easy, saving time and significantly reducing initial set-up costs. At the same time, the MIPP contributes to greater reliability with easier and more efficient system management that requires less maintenance. With a lightweight aluminum structure that increases its overall versatility, the MIPP easily mounts on a DIN Rail or on the sides of cabinets using a wall mount plate. The small housing, high port density and modularity keep cabinet space to a minimum.
The MIPP was designed for industrial use, where its functionality and reliability can make a significant contribution to the uptime and availability of systems. It is ideal for use in a wide range of industrial applications requiring maximum system reliability and flexibility. The industrial design makes it highly suited for use in machine building, transportation, alternative power generation, power transportation and distribution and oil and gas markets, as well as for general use in commercial buildings and other applications.
For the first time, MIPP’s unique modular design and compact dimensions allow up to six individual modules to be combined in any permutation to create a large single patch panel where fiber and copper cables can be connected at the same time. When required, each module is easily removed or replaced for maximum system flexibility.
The MIPP is available as both single and double modules:
6 x SC duplex adapters (up to 12 fiber connections)
6 x LC duplex adapters (up to 12 fiber connections)
4 x RJ45 keystone jacks
12 x SC duplex adapters (up to 24 fiber connections)
12 x LC duplex adapters (up to 24 fiber connections)
Frank Wei, director of marketing for Hirschmann said, “The MIPP is a completely new solution that combines copper and fiber, an industry first. Installation is quick and easy, saving time and significantly reducing initial set-up costs. At the same time, its functionality contributes to greater reliability and easier and more efficient system management that requires less maintenance.”
Hirschmann brand means dependable signal transmission – even in harsh industrial environments. The Hirschmann brand represents experience and expertise in automation technology, developed since pioneering the development of Ethernet as a common standard for industry networks. Today, Hirschmann products will ensure hassle-free and secure data communication under the toughest conditions. The high transmission speeds and large bandwidths ensure the fastest possible processing of large amounts of data. For more information on Hirschmann’s New Modular Industrial Patch Panel, download Product Bulletin 334 or contact Hirschmann, a Belden Brand, at 1540 Orchard Drive, Chambersburg, PA 17201, Telephone: 1.719.217.2299. Fax: 719.217.2279.
St. Louis-based Belden Inc. designs, manufactures, and markets cable, connectivity, and networking products in markets including industrial automation, enterprise, transportation, infrastructure, and consumer electronics. It has approximately 6,800 employees, and provides value for industrial automation, enterprise, education, healthcare, entertainment and broadcast, sound and security, transportation, infrastructure, consumer electronics and other industries. Belden has manufacturing capabilities in North America, South America, Europe, and Asia, and a market presence in nearly every region of the world. Belden was founded in 1902, and today is a leader with some of the strongest brands in the signal transmission industry. For more information, visit www.belden.com.