Solutions for Healthcare

Healthcare facilities can benefit greatly from a converged infrastructure. As the foundation for all communications, a converged infrastructure ties all healthcare applications and systems together along one or more infrastructures. It provides the bandwidth and signal performance required by all of the systems and applications used in healthcare facilities today and is scalable to meet the requirements for emerging systems such as picturing archiving and communications systems (PACS), computer-based practitioner order entry (CPOE) and clinical decision support systems (CDSS).

(object placeholder)

And no one is more qualified than Belden for navigating the evolving healthcare applications landscape and the migration to a converged communication infrastructure. We are uniquely capable of supporting several different communication infrastructures – no matter where you are in the convergence process because we offer such an extensive product portfolio that includes:

From legacy-based infrastructures to fully converged IP-based infrastructures, we understand the information flow, transmission technologies, obstacles and efficiencies involved in making convergence a reality. In fact, there are over 2,000 Belden Certified healthcare facilities throughout North America using Belden products in their communication infrastructure.

Find out how others in the Healthcare market have benefited from using Belden solutions.

Downloadable Resources

Copper Catalog
Fiber Catalog
Infrastructure Solutions Catalog
Commercial AV Solutions Guide