Dark purple streak waves on purple background
Related Tags

St. Louis, Missouri – August 28, 2025 – Belden Inc. (NYSE: BDC), a leading global provider of complete connection solutions, today announced the launch of several new products designed to enhance performance, security and reliability across automation and smart infrastructure environments.

  • Belden Gel-Free Loose Tube Optical Fiber Cables feature a compact, resilient design for robust connectivity while eliminating the hassle of messy gel compounds. These cables resist moisture intrusion and ensure long-term durability in demanding operational settings. Available in the EMEA region.

  • Belden Classics Essential-Lite - LSZH IEC-EN Rated Cables offer enhanced analog and serial data performance, along with a Low Smoke Zero Halogen rating for standard indoor environments.

  • Belden RemoteIP OSP Cables feature a cost-effective, simplified construction and easy deployment. Belden’s RemoteIP OSP cables extend Ethernet channel distances up to 215 meters while maintaining low heat levels and minimal power loss. This new addition to the RemoteIP line is fully compatible with REVConnectTM connectivity.

  • The Belden Industrial Firewall IAF-240 provides scalable, multi-layered protection for critical OT networks. It combines deep visibility, threat prevention and high availability in a compact, industrial-grade design built to reduce risk and downtime.

  • Version 1.11 of Belden PROVIZE Suite network planning and commissioning software introduces new features, including network planning support for the GREYHOUND2000 switch. PROVIZE Explorer has a new MultiConfig feature, allowing users to update the firmware of multiple devices at once, saving time. Further improvements ease planning and commissioning even more.

  • Hirschmann BOBCAT Switches are now certified to comply with IEC 62443-4-2 Security Level 2 functional requirements. This IEC standard addresses security in industrial automation and control systems.

 

Learn more about these products, as well as the technologies and applications they support.

 

About Belden

Belden Inc. delivers complete connection solutions that unlock untold possibilities for our customers, their customers and the world. We advance ideas and technologies that enable a safer, smarter and more prosperous future. Throughout our 120+ year history we have evolved as a company, but our purpose remains – making connections. By connecting people, information and ideas, we make it possible. We are headquartered in St. Louis and have manufacturing capabilities in North America, Europe, Asia and Africa. For more information, visit us at www.belden.com; follow us on FacebookLinkedIn and X/Twitter.

 

For more information, contact:

Mary Melchiorre
Manager, Corporate Marketing Communications
+1-514-207-6106
[email protected]

 

Belden and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.