- Home - Belden.com
- About Belden
-
Market Solutions
-
Products
-
Resource Center
Here are a few of Belden’s most notable system technology innovations in recent years.
IBDN System 10GX – In today’s data center and LAN environments, the newest performance challenge lies in providing 10 Gb/s transmission speeds over copper-based, 4-pair channels – a ten-fold performance increase over previous generation channels. Most manufacturers have attempted to meet this 10-fold increase by ‘pumping up’ or strengthening traditional product design elements, typically with disappointing or marginal results. Belden took a whole new approach by inventing unique, new enabling technologies to meet the 10 Gb/s challenge.
Here are the key technology innovations developed for Belden’s IBDN 10GX System:
RoundFleX Cable Design – a design which optimizes pair twist lays and increases and randomizes the distance between pairs in a cable and its neighboring cables, so both ANEXT and AFEXT coupling are improved. This unique cable design is also smaller, more flexible and more installer-friendly than other Category 6A cables.
FleXPoint PCB Technology – a technology innovation which utilizes a flexible printed circuit board within the module that allows the compensation circuitry to be located directly at the point of plug contact. This reduces the delay between the source of the crosstalk in the plug and the crosstalk cancellation circuitry on the PCB, resulting in a dramatic reduction in crosstalk at frequencies up to 625 MHz.
MatriX IDC Technology – a patent-pending IDC design and patch panel circuit layout which positions each IDC at 90 degrees to its neighbor – effectively canceling out the Alien Crosstalk between modules by 15dB as compared with traditional technology.
X-Bar Installation Device – a control device that affixes to the module to enable the accurate positioning of each UTP pair for termination on the 10GX Module's IDC pins. This enables installers to maintain the proper conductor twist lays during installation to prevent untwisting. This assures Installable Performance, the after-installation assurance that no termination errors have been committed.
Throughout its history, Belden has developed some of the most innovative and high-performance cable designs and constructions in the industry. Two notable designs include Bonded-Pair Cables and Banana Peel Composite Cables, while the following shielding innovations – Beldfoil, Duofoil, “French Braid” and Z-Fold – were developed to meet the market demand for more effective cable shields.
Bonded-Pair Cables – a patented design that bonds the individual insulated conductors of each pair along the full length of the cable. This bonded construction delivers Installable Performance. That is, Bonded-Pair cables are consistent in the distance between the conductors and in the amount of twist, throughout the installation process, so they deliver the same superior – and stable -- electrical performance both before and after the cable's installation. Bonded-Pair cables are also used in the manufacture of Belden's CAT6+ and CAT5E Bonded-Pair Modular Patch Cords, where this technology ensures that the cords meet the stringent TIA mechanical stress reliability specifications.