Sometimes Projects Can’t Wait on Materials to Arrive

There are timelines to beat, clients to keep happy, last-minute changes that happen or things overlooked during planning. That’s why Belden is working with our distributors to launch a new same-day shipping service for its fiber cable and connectivity solutions. There are no minimum or maximum orders on eligible products, so you can get exactly what you want, when and where you want it.   

Here’s how it works:

  • Place an order of eligible products with your preferred Belden Distributor, specifying same-day shipping

  • Specify shipping method and provide a shipping account number (UPS, FedEx, etc.)

  • Your order will ship that same day!

  • Cut-off times apply; please contact your preferred Belden Distributor for details.  

*See Terms and Conditions Below


Fiber Same-Day Shipping Eligibility

  • FX Fiber Distribution Cable

  • Standard FX Patch Cords

  • FX Pigtails

  • FX Fusion splice-on connectors

  • FX ECX

FX Fiber Distribution Cable

# of Fibers OM3 OM4 OS2
Non-unitized Plenum – Indoor
6FI3D006P9FI4D006P9FISD006P9
12FI3D012P9FI4D012P9FISD012P9
24FI3D024P9FI4D024P9FISD024P9
Non-unitized Plenum Armor – Indoor
6FI3D006A9-FISD006A9
12FI3D012A9FI4D012A9FISD012A9
24-FI4D024A9FISD024A9
Unitized 12-Fiber Sub-Units Plenum – Indoor
48-FI4D048PKFISD048PK
Unitized 12-Fiber Sub-Units Plenum Armor – Indoor
48-FI4D048AKFISD048AK
Non-unitized Plenum – Indoor/Outdoor
6FD3D006P9FD4D006P9FDSD006P9
12FD3D012P9FD4D012P9FDSD012P9
24-FD4D024P9FDSD024P9
Non-unitized Plenum Armor – Indoor/Outdoor
6FD3D006A9FD4D006A9FDSD006A9
12FD3D012A9FD4D012A9FDSD012A9
24-FD4D024A9FDSD024A9
Unitized 12-Fiber Sub-Units Plenum – Indoor/Outdoor
48--FDSD048PK
Unitized 12-Fiber Sub-Units Plenum Armor – Indoor/Outdoor
48--FDSD048AK

Standard FX Patch Cords

Description Length Fiber Type Part Number
LC Duplex Uniboot to LC Duplex Uniboot 2 m OM4 (Erika Violet) FP4LULU002M
3 m OM4 (Erika Violet) FP4LULU003M
OS2 (Blue/Yellow)FPSLULU003M
LC Duplex to LC Duplex 2 m OM3 (Aqua)FP3LDLD002M
OM4 (Erika Violet)FP4LDLD002M
OS2 (Blue/Yellow)FPSLDLD002M
3 m OM3 (Aqua)FP3LDLD003M
OM4 (Erika Violet)FP4LDLD003M
OS2 (Blue/Yellow)FPSLDLD003M

FX Pigtails

Description Connector Type Fiber Type Part Number
Standard Pigtail Kits (Connector on 900um Fiber)  LCOM3FT3LC900PR12
OM4FT4LC900PR12
OS2 -
Standard Single Pigtails (Connector on 900um Fiber)OM3FT3LC900PS01
OM4FT4LC900PS01
OS2FTSLC900PS01

FX Fusion Splice-On Connectors

Description Fiber Type Part Number
LC with 900/250 μm Boot, 1/Pack Multimode - OM3/OM4 - AquaFT3LC900FS01
Multimode OM4 - Erika VioletFT4LC900FS01
Single-mode OS2 - BlueFTSLC900FS01
LC with 2 mm Boot, 1/PackMultimode - OM3/OM4 - AquaFT3LC2MMFS01
Multimode OM4 - Erika VioletFT4LC2MMFS01
Singlemode OS2 - BlueFTSLC2MMFS01

FX ECX Housings

Description Total LC Duplex using ECX Frames Total LC Duplex using ECX Cassettes Part Number
1U Housing - 2 Cassettes or Frames 32 24ECX-01U
4U Housing - 12 Cassettes or Frames 192 144ECX-04U

Standard FX ECX Frames

Description Fiber Type Part Number
LC Duplex 12(24) OM3 (Aqua Adapters)FF3X12LD
OM4 (Erika Violet Adapters)FF4X12LD
OS2 (Blue Adapters)FFSX12LD

*Terms & Conditions

  1. Available in the US and Canada only.
  2. Orders must be for eligible, in-stock products. It is Belden’s expectation that it will be able to offer same-day shipping on all eligible products. However, Belden cannot guarantee that its inventory of eligible products will always allow for same-day shipping of all orders. If we are unable to fulfill an eligible order for an eligible product on the day received, we will inform the customer and, if possible, offer potential alternatives. 
  3. Installer specifies shipping instructions, time-frame and method with Distributor.
  4. All orders must be accompanied by a shipping account name and number. All shipping charges will be billed to the provided shipping account number. Shipments will be shipped to the delivery address identified when the order is placed using the shipping method identified at the time of the order. 
  5. All sales made under this program shall be subject to Belden’s Standard Terms and Conditions of Sale (the “Standard Terms”), with the exception of shipping charges, which will be billed to the account provided.
Resources
Eligibility Sheet

Questions?

Call us at 800-BELDEN1!