News Release

Belden Launches Hirschmann BXP (BOBCAT eXtreme Performance) Managed Switch

Belden
Compact, Ruggedized EN 50155 Switch for Railway Rolling Stock.

 

St. Louis, Missouri – February 21, 2024 – Belden Inc. (NYSE: BDC), a leading global supplier of network infrastructure and digitization solutions, today announced the launch of its Hirschmann BXP (BOBCAT eXtreme Performance) managed switch. This extension of the proven BOBCAT switch family from Hirschmann, a Belden brand, offers a compact design, enhanced flexibility and interoperability, and speeds of up to 10 gigabits per second (Gbps) to meet the dynamic needs of railway rolling stock applications.

 

As train builders and operators look to connect more onboard equipment – including data-intensive, high-speed cameras and internet devices – they need a strong network backbone to provide continuous uptime and accurate data transmission. With its powerful combination of features, including a compact footprint, high port count, up to 10 Gigabit Ethernet (GE), Power over Ethernet (PoE++), and protocols like high-availability seamless redundancy (HSR) and parallel redundancy protocol (PRP), the ruggedized BXP can withstand harsh environments on moving trains.

 

The BOBCAT managed switch provides powerful benefits, such as:

  • High port density, including 20-port and 28-port variants, to connect more network devices.

  • Robust bandwidth and speed with up to 6x 10 GE ports, future-ready for expansion.

  • PoE ++ up to 120 W to meet the high power demands of onboard devices.

 

“The BXP is the first BOBCAT switch designed for the specific requirements of railway rolling stock with unique features like the highest port density and fastest speeds in our portfolio,” said Santosh Chandrashekhar, Product Manager. “BXP adds value through simplified web-based configuration, flexible Layer 2 or Layer 3 switch configuration options, and advanced security via the Hirschmann Operating System (HiOS). With its combination of high port counts, PoE++ and low maintenance requirements, the BXP also delivers low total cost of ownership.

 

The BXP managed switch meets essential railway rolling stock standards, such as European Standards EN 50155 and EN 50121 and EN 45545, for shock, operating temperature, electromagnetic interference, vibration, fire resistance and other conditions. The BXP has attained multiple international and industry certifications – including Conformité Européenne (CE), International Electrotechnical Commission (IEC), and Registration, Evaluation, Authorisation and Restriction of Chemicals (REACH). 

 

About Belden

Belden Inc. delivers the infrastructure that makes the digital journey simpler, smarter and secure. We’re moving beyond connectivity—from what we make to what we make possible through a performance-driven portfolio, forward-thinking expertise and purpose-built solutions. With a legacy of quality and reliability spanning 120-plus years, we have a strong foundation to continue building the future. We are headquartered in St. Louis and have manufacturing capabilities in North America, Europe, Asia and Africa. For more information, visit us at www.belden.com; follow us on Facebook, LinkedIn and Twitter.

 

For more information, contact:

Scott Todd
Marketing Communications Manager
(317) 316-6473
[email protected]

 

Belden and the Belden logo are trademarks or registered trademarks of Belden Inc. or its affiliated companies in the United States and other jurisdictions. Belden and other parties may also have trademark rights in other terms used herein.